Regal Introduces Enhanced JuggerNaut<sup>&reg;</sup> Condenser Fan Motor Lineup

Juggernaut Pro

Improved bearings and D-133 Inverter Duty Wire help increase operational efficiency


BELOIT, Wis., June 27, 2019 — Regal Beloit Corporation, a leading manufacturer of electric motors, electrical motion controls, power generation and power transmission components, announced it will debut a series of upgrades to its JuggerNaut motor line, released under the Century® brand. The JuggerNaut motor lineup features the upgraded Century JuggerNaut motor and the new Century JuggerNaut Pro motor with bearing current protection (BCP).

The Century JuggerNaut motor now functions with a non-conductive grease and features full-phase insulation. The Century JuggerNaut Pro motor with BCP, which will be released soon, will also feature MaxGuard® insulation as well as carbon brush technology that minimizes induced shaft voltage. Both motors feature D-133 inverter duty wire, which helps in the reduction of bearing currents. 

“Regal continues to innovate its products to provide customers with the most efficient products on the market, with options on two levels: better and best,” said John Calloway, distribution product marketing manager, Regal. “The product level depends on a customer’s operational needs, but all upgrades enable longer bearing life and longer motor life with each option, which ultimately leads to more efficient operations by decreasing downtime.

The Century JuggerNaut motors feature:

  • Quick-connect designs
  • Automatic reset thermal protectors
  • Non-conductive grease bearings
  • Double-sealed ball bearings
  • Class F insulation
  • 70°C (158°F) ambient temperature
  • Voltage Change Device (VCD) to quickly change voltage on the spot

The Century® JuggerNaut® Pro motor with BCP offers:

  • 70°C (158° F) ambient temperature
  • Enclosed shaft end bracket with vented frame
  • Automatic reset thermal protector
  • External shaft slinger
  • A threaded lead exit
  • Voltage Change Device (VCD) to quickly change voltage on the spot
  • Double-sealed ball bearings 

The motor line is meant for commercial and residential fan/heat pump applications and may be installed outdoors. The motors need to be mounted within the airflow of the fan for proper cooling. All three improved motors offer upgrades that allow for longer operating life for bearings and motors as well as cooler and smoother operation. 

About Regal Beloit Corporation
Regal Beloit Corporation (NYSE: RBC) is a leading manufacturer of electric motors and controls, power generation products and power transmission products serving customers throughout the world. We create a better tomorrow by developing and responsibly producing energy-efficient products and systems. Our company is comprised of three operating segments: Commercial and Industrial Systems, Climate Solutions and Power Transmission Solutions. Regal is headquartered in Beloit, Wisconsin and has manufacturing, sales and service facilities worldwide. For more information, visit RegalBeloit.com
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
This item is discontinued, but you may order against the remaining inventory. You have requested {4} items of the total remaining quantity of {2}.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.