Regal Beloit is now Regal Rexnord. Click here to learn more.

New Department of Energy (DOE) Pool Pump & Motor Regulations

Department of Energy (DOE) Legislation

In January 2017, the DOE established the first national energy efficiency standards for Dedicated Purpose Pool Pump (DPPP) regulations. This standard impacts most in-ground pools by requiring variable-speed technology. Pumps for smaller in-ground pools, pumps for above ground pools, and pressure cleaner booster pumps can continue to be single-speed.

For a few hours each day, pool pumps need to operate at a high speed to provide a high flow rate for mixing and cleaning. However, much of the time, the pump just needs to circulate the pool water through the filtration system at a low flow rate. According to the DOE, the use of variable-speed pumps can reduce energy usage by about 70% compared to single-speed pumps as they can operate at a lower speed for the rest of the day when the pump is just circulating water for filtration.

Replacement Pool Pump Motors

A pool pump motor could fail before the variable speed DPPP needs to be replaced. The concern is whether an unknowing homeowner or contractor might replace it with a single-speed replacement motor, which would negate the benefits of the variable speed pump.

A dedicated purpose pool pump (DPPP) motor covers any motor that is certified to UL 1004-106 and/or designed or marketed for use in DPPP motor replacement. This applies to motors manufactured domestically or imported. The scope would exempt six types of pool pump motors — polyphase motors capable of operating without a drive (and distributed in commerce without a drive), waterfall pump motors, rigid electric spa pump motors, storable electric spa pump motors, integral cartridge-filter pool pump motors and integral sand filter pool pump motors. These exemptions align with the DPPP standards.

Impacts to Homeowners and Distributors

In July 2021, new pool installations and replacement DPPP will require a variable speed pump and motor. According to the DOE, variable speed pumps can reduce energy usage by about 70 percent relative to single-speed pumps by operating at a lower speed when the pump is circulating and filtering water. While the variable speed pumps may have a higher initial cost, its energy efficient operation will provide payback. The DOE estimates average life-cycle cost savings for owners of in-ground pools of $2,140 with a payback of less than one year.

When the new regulation takes effect in July 2021, manufacturers will be transitioning and selling based on the new regulations, but existing inventory of non-compliant pumps are still permitted to be sold and installed. Replacement variable speed motor legislation is still pending and is discussed in detail below.



Status of the Pending Legislation

Department of Energy (DOE)

The next step is for the DOE to adopt the stakeholder recommendations and issue a Direct Final Rule. Enacting this legislation would effectively close the replacement motor “loophole”. This would set a prescriptive standard that all pool pump motors on the market must meet, regardless of whether they are being sold with a new pool pump or as a replacement. The anticipated DOE “Motor Rule” is likely to be effective in 2022, however the effective date is uncertain. This approach ensures that customers will benefit from the variable speed motor technology that is projected in the upcoming 2021 pool pump standard.


California Energy Commission (CEC)

CEC Title 20 Section 1605.3(g)(5) requires any motor used for residential filter pump applications and manufactured before July 19, 2021 that is greater than or equal to 1.0 THP be replaced with a two-speed or variable speed motor. Effective July 19, 2021 CEC Title 20 1605.3(g)(6) requires any motor used for replacement dedicated-purpose pool pump motor on all residential and commercial applications and manufactured on or after July 19, 2021 that is greater than or equal to 0.5 THP be replaced with a variable speed motor.

 


Outline for Pool Pump Motors UL 1004-10 Requirements for DPPP Motors

 

 

Brands
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
This item is discontinued, but you may order against the remaining inventory. You have requested {4} items of the total remaining quantity of {2}.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.