Imagine this scenario. You are on a service call and have determined that the failed motor is an OEM ECM motor. Before Evergreen® replacement motors were available, the only replacement for ECM motors was through the HVAC equipment OEM. If the HVAC OEM happens to have the motor in stock, you will drive to the OEM distributor to pick up the motor, drive back to the job and install the motor. If the HVAC OEM does not have the motor in stock or is not local, it may take up to a week or more to receive the replacement ECM. In most of these scenarios, you are not going to get the replacement motor the same day as the repair. Now consider this. If the average travel time to go get an OEM motor is one hour, and the average truck replaces two motors per week, you are losing two hours per week. If the operating cost of your truck is $100 per hour, you could be spending $200 per week, which equates to over $10,000 per year, per truck, driving to get parts.
Luckily, there is a better way. Instead of OEM parts inventory, you can use Evergreen® EM and VS motors and carry the correct motors on your truck today. Evergreen motors on the truck means you get the job done in one call, without any added trips to the distributor.
Evergreen EM and VS motors replace millions of OEM ECM indoor blower motors. Evergreen replacement motors will save you time, lower your inventory, and allow for easy installation.
Evergreen VS motors replace constant airflow ECM (often referred to as variable speed indoor blower motors) built by Genteq® and formerly branded GE® products. With the Evergreen VS motor, you can now replace millions of OEM ECM motors the same day, without the need to drive to each HVAC OEM to get the motor. The Evergreen VS motor is a drop-in replacement that is compatible with both 16-pin and 4-pin variable speed designs. These motors are pre-programmed and ready to use out of the box.
Evergreen EM motors replace constant torque ECM indoor blower motors such as Genteq X13® and Endura® Pro motors, US Motors® SelecTech® and RESCUE SELECT®, and Broad Ocean Motors® with 24 VAC speed taps. Again, this means you can also replace millions of constant torque OEM ECM motors the same day, without the need to drive to each HVAC OEM to get the motor. The Evergreen EM motor is a drop-in replacement that is compatible with the standard 9-pin plug used by most constant torque ECM manufacturers. These motors are pre-programmed and ready to use out of the box.
The following are believed to be the trademarks and/or trade names of their respective owners and are not owned or controlled by Regal Rexnord Corporation.
GE: General Electric Company; Broad Ocean: Zhongshan Broad-Ocean Motor Co., Ltd.; US Motors, SelecTech and Rescue Select: Nidec Corporation
Browse our Catalog
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.