Jaure

 

GENERAL INDUSTRY DRIVES

THE MOST SUITABLE JAURE COUPLING FOR ANY APPLICATION

 Couplings  
 MT Compact Gear Coupling  JFTL Torque limiters to protect the drive train from peak torques 
 BARFLEX® Barrel Coupling for cranes and hoisting applications  JCFS & JGFS Carbon & glass fiber drive shafts
 LAMIDISC® Non lubricated torsionally stiff disc pack coupling  JHC Hydraulic shaft coupling. Components & Solutions
 MAX-C® Non-lubricated high torque capacity resilient coupling  JAUFLEX® Non lubricated elastomeric coupling
 RECORD Lubricated flexible grid coupling  IXILFLEX® Bidirectional rubber link coupling for high misalignment
 Components & Solutions  
 JS NUT Multi-Jack bolt tensioner  Electronic Wear Indicator Remote monitoring of the coupling wear
 GREASE Bidirectional rubber link coupling for high misalignment  
  

No matter the application (cranes & hoisting, paper, minerals, etc.) in need of a flexible coupling, our extensive product portfolio allows us to meet any requirement. Both standard and engineered-to-order coupling solutions are available. We can provide a turnkey solution for a complete drive, ensuring that all of our solutions are tailored to each application.

 

Our sales and technical representatives will be glad to assist you.

 

 

CRANES & HOISTING

JAURE BARREL AND GEAR COUPLING

BARFLEX TCBR barrel couplings for hoisting and JAURE MTFS gear coupling with brake disc.

Barrel Coupling

 

 

Jaure barrel couplings are recommended for installation in crane lifting mechanisms.

 

To use a barrel coupling instead of a gear coupling will bring a significant decrease of the space needed for coupling. Besides, barrel couplings are subjected to much lower bending stress on the root of the teeth and the increased safety factor is obtained against peak radial loads.

 

 

 

JAURE DISC PACK AND ELASTIC COUPLING

Maintenance-free SXFD LAMIDISC All-steel disc pack and SDDL JAUFLEX elastic couplings.

Compolink

 

We also provide the coupling between the main engine and the gearbox input shaft. Various types of flexible couplings, MT gear, LAMIDISC disc pack and JAUFLEX elastic with brake disc or drum couplings are delivered according to customer requirement.

 

An electronic wear indicator feature is also available. This feature allows the user to monitor wear remotely. Thousands of Jaure barrel couplings are successfully operating for years in various demanding applications such as container cranes, ladle cranes in steel mills, rubber gantry cranes, traveling cranes for industry applications, etc.

 
 

PULP & PAPER

JAURE GEAR COUPLING

Heavy-duty types MTG-HD-NT and MTGX-HD-NT with nitrided gears.

JAURE JAURE

 

Our company is a global supplier of flexible couplings to customers in the pulp and paper industry.

 

For over 40, years Jaure MT gear couplings have been successfully operating in various lines for the processing of fiber pulps, paper, board and tissue machines. 

 

MT gear couplings are the most compact solution for critical applications that demand high torque transmission. As an example, engineered-to-order Jaure heavy-duty type MT-HD gear couplings are running in some world’s biggest refiners.

 

JAURE DISC PACK COUPLING

Maintenance-free All-steel LAMIDISC disc pack ranges: DO Drop Out style and CC-E with a split spacer.

LamiDisc

 

The Jaure LAMIDISC disc pack coupling was later introduced to retrofit gear couplings in the production of paper. LAMIDISC couplings are designed to operate with no maintenance required. It, therefore, allows the paper mills to eliminate downtime for maintenance and advances towards a lubrication-free plant environment.

 

These couplings are used in the two main areas of the paper machine: the wet area and the drying end. Thousands of LAMIDISC couplings are running in various processes of paper production such as presses, dryers, pumps, calendars, reels, roll handling, etc. Our standard program of LAMIDISC couplings is adapted to each application need in terms of spam, dynamical balancing, electrically insulating, painting, or any other specific request.

 

MINERALS & MINING

JAURE GEAR COUPLING AND MULTI-JACK BOLT TENSIONER

Heavy-duty type MTG-HD gear coupling and JS nut multi-jack bolt tensioner.

JAURE

 

Backed by extraordinary technological capabilities and resources, we deliver customized heavy-duty solutions to the most demanding sectors like minerals and mining processing. 

We have an extensive product portfolio of flexible couplings, both torsionally rigid and elastic. 

Jaure heavy-duty MT-HD gear and record grid couplings are made to order to meet the needs of the most demanding mill drives (Ball, SAG, etc.). 

 

JAURE GEAR COUPLING

MTES disengaging designs with a lever, screw-jack, etc.

JAURE

 

JAURE COMBINED DISC PACK AND ELASTIC COUPLING

LAMIDISC SX with MAX-C rubber in shear couplings.

 

Auxiliary inching drives are also running with Jaure MTES disengaging couplings. 

 

Manual, pneumatic or hydraulic levers are also delivered on demand. 

 

To meet other needs in the mills like torsional damping, dusty atmospheres or reducing downtime for maintenance, we have a product portfolio of non-lubricated couplings such as LAMIDISC all-steel disc pack or Jaure/Kop-Flex® Max-C.

 

PETROCHEMICAL / OIL & GAS

JAURE DISC PACK AND GEAR COUPLING

DOAE LAMIDISC coupling with electrical insulation and MTNAE gear coupling with electrical insulation.

LamiDisc

JAURE

 

We have a wide variety of products for use in the oilfield industry. Common solutions include a variety of MT gear couplings and LAMIDISC disc pack couplings which can be customized for vertical installation, electrical insulation, various spans, etc.

 

Various executions of Jaure couplings meet the requirements of the American Petroleum Institute (API 610 and API 671) and can be also ATEX certified on demand.

 


 

 

COOLING TOWERS / MACHINE TOOLS

JAURE COMPOLINK® AND COMBINED DISC PACK COUPLING

Composite link coupling and LAMIDISC disc pack coupling in combination with JGFS glass fiber and JCFS carbon fiber spacers.

 

Jaure composite shaft lines JGFS-glass fiber & JCFS-carbon fiber are combined with Jaure® flexible couplings, for installation in high humidity and corrosive atmospheres like cooling towers, for example. These shafts are also used for higher speed applications such as machine tools and test benches.

 

SERVICE

POWERLIGN® COUPLINGS TORQUE MONITORING

JAURE

 

To reach desired low operating costs and avoid unscheduled shutdowns, proper drive maintenance is key. Our gear couplings can be repaired for much less than the cost of new ones, and proper maintenance extends the life of the equipment. 

 

Regal has an experienced and skilled service team to provide worldwide support of its Jaure and Kop-Flex brands. It is available to share its expert assistance in designing a predictive and preventive maintenance program.

 

TORQUE MONITORING

KOP-FLEX COUPLING GREASES

JAURE

 

Torque monitoring is a valuable tool for preventative maintenance and problem-solving. It provides real-time data to the mill operators. 

 

Main purpose: 

  • Understanding the real loads under working conditions versus design loads. 
  • Definition of overload protection devices if needed. 
  • Definition of the most appropriate coupling solution. 
  • Effect of transient loads on the coupling.
     

JAURE MANUFACTURING PROGRAM

 

Jaure

 

JAURE

 

KOP-FLEX® & JAURE® COUPLINGS MANUFACTURING PROGRAM

 

JAURE
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
This item is discontinued, but you may order against the remaining inventory. You have requested {4} items of the total remaining quantity of {2}.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.
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
BROW,DUR,FJ,GRVG,HUBC,JAURE,KOPF,MS,MCGI,MW,MORS,ROLW,SLMS,SP,ADDX,AG,BERG,BH,CAR,CES,CNTA,DURA,EFLX,FALK,HIGH,KRO,LINK,MAR,MB,MCC,OMEG,PSI,REX,RPT,SHA,SIM,STE,TAP,THOM,TLK,TRUE,TUF,VIVA,WRAP,LNKB,RXND,MARB