Regal<sup>®</sup> Introduces System Plast<sup>®</sup> iCOF<sup>®</sup> Condition Monitoring Device
BELOIT, Wis., Aug. 11, 2020 — Regal Beloit Corporation, a leading manufacturer of electric motors, electrical motion controls, power generation and power transmission components, announced the introduction of its new System Plast® iCOF® condition monitoring device for food and beverage conveyor lines.
For manufacturers running a manufacturing line, especially a dry running line, friction is a key factor for the proper handling and flow of containers. The iCOF condition monitoring device is designed to monitor the condition of a manufacturing line or a part of it by measuring the coefficient of friction (COF) of a chain or belt while it is running. It returns the average value and trend of the COF. The goal is to maintain line efficiency and an optimum cleaning regime.
“The iCOF device can be used in any conveyor, where a stable friction is the critical point. In dry lines, this value can more easily be affected by several factors, including the cleaning conditions of the conveyors,” said Brad Gossard vice president and general manager, PTS Conveying, Regal. “Inliners, feeders or the points where the containers change their speed quickly are the areas to watch. The iCOF condition monitoring device can also be used in mass conveyors to keep the back-line pressure under control.”
The iCOF device can be mounted on a conveyor and integrated in the line control system. Without any operator intervention, the system will independently measure the friction at regular intervals. With these data, it is possible to calculate an average value and the related trend and set alerts to take corrective action.
The iCOF condition monitoring device is compatible with Profinet protocol and Ethernet. The iCOF design fits with standard 85 mm pitch conveyors. Its compact and firm structure, made in high strength steel (AISI 304), is completely closed and waterproof, offering the best resistance to cleaning agents. The easy and quick replacing of wear parts, a low tension and current absorption (24 V, 400 mA, 10 W) ensure reliability and operability.
The iCOF system includes the iCOF device, one slider to imitate product type (PET, CAN or GLASS), one set of screws for the slider, one screwdriver, and one USB drive with graphical user interface (GUI). For more information, visit the iCOF product page today.
About the Company
Regal Beloit Corporation (NYSE: RBC) is a global leader in the engineering and manufacturing of electric motors and controls, power generation products and power transmission components, serving customers throughout the world. We create a better tomorrow by developing and responsibly producing energy-efficient products and systems.
Our company is comprised of four operating segments: Commercial Systems, Industrial Systems, Climate Solutions and Power Transmission Solutions. Regal is headquartered in Beloit, Wisconsin, and has manufacturing, sales and service facilities worldwide.
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.