How Gear Ratio Factors in the Choice for an Inverter Duty Motor



Electric motors are essential components in all types of industries. No matter the industry, selecting the right electric motor for the application is important.

Choosing a motor requires considering factors like torque requirements, speed, efficiency, and the desired gear ratio. Gear ratio indicates the relationship between the rotational speeds of a motor’s input and output shafts. Usually expressed as 1000:1 or 2000:1, gear ratio is used to adjust the speed and torque characteristics of the motor. This guide can help you decide whether a 1000:1 or a 2000:1 electric motor is right for you.

Understanding Gear Ratio

The gear ratio of an electric motor is the ratio between the number of teeth on the input gear and the number of teeth on the output gear. For gears, the motor drives the input gear, while the output gear is connects to the load.

A higher gear ratio means more torque and less speed, while a lower gear ratio provides higher speed and lower torque. The choice between a 1000:1 or a 2000:1 gear ratio motor depends on the specific requirements of the application.

When to Choose a BlackMAX® 1000:1 Electric Motor

  • Heavy Loads. If your application involves moving heavy loads, a 1000:1 gear ratio motor can provide the necessary torque to handle the weight effectively. For instance, in industries such as construction or material handling, where heavy lifting is involved, a 1000:1 motor is often suitable.
  • Low Speed Applications. Certain applications require precise and slow movements. A 1000:1 motor offers a higher torque output, enabling the motor to maintain steady motion at low speeds. Examples include conveyor systems, robotic arms, or machines that require precise positioning.
  • High Reduction Requirements. In some cases, the application may demand a high reduction ratio to achieve the desired output. A 1000:1 gear ratio motor can efficiently reduce the input speed to the required level while delivering sufficient torque to drive the load.
  • Extended life under thermal and dielectric stress. Rapid switching can cause increased power losses in the motor windings, resulting in heat generation. The heat generated during each switching cycle adds up over time and can raise the overall temperature of the motor and can cause voltage spikes and high-frequency harmonics in the motor windings. These voltage spikes and harmonics can stress the insulation system of the motor. Our MAX GUARD® insulation system delivers long, dependable motor life under these conditions
  • Space Constraints. If your application has limited space for the motor and the gearbox, a 1000:1 gear ratio motor might be preferable. Since it provides a higher torque output, it may eliminate the need for additional mechanical components, allowing for a more compact and streamlined design.

BlackMAX 1000:1 Inverter Duty Motors provide high energy savings, constant torque speed range operation and several other benefits.

When to Choose a BlueMAX® 2000:1 Electric Motor

  • Extremely Heavy Loads. When dealing with exceptionally heavy loads, such as in large-scale industrial machinery or heavy-duty cranes, a 2000:1 gear ratio motor may be necessary. The higher torque output allows the motor to handle the increased weight effectively.
  • Ultra-low Speed Applications. For applications requiring an extremely slow rotational speed, a 2000:1 motor can provide the necessary torque while maintaining a consistent pace. This is crucial in applications like precision manufacturing or delicate operations where even minor speed fluctuations can lead to errors.
  • Precise Positioning. Certain applications demand precise positioning with minimal backlash. A 2000:1 motor can offer the required accuracy and stability, ensuring precise movements and eliminating unwanted deviations.
  • Extended life under Thermal and Dielectric stress. Marathon BlueMAX Motors are insulated with Our MAX GUARD® insulation system who delivers a long motor life under stress.

BlueMAX 2000:1 Inverter Duty Motors excel in commercial and industrial applications around the world.

Finding the Right Gear Ratio For Your Application

Selecting the appropriate gear ratio for an industrial motor is essential to ensure optimal performance in specific applications. Choosing between a 1000:1 or a 2000:1 gear ratio motor depends on the task's requirements.

A 1000:1 motor excels in heavy load applications, low-speed operations, and high reduction requirements. On the other hand, a 2000:1 motor is suitable for extremely heavy loads, ultra-low speed applications, and precise positioning needs.

Understanding the demands of your application and consulting with our experts can help you make an informed decision to ensure your Motor to Get the Job Done.




Talk To Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business. 
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
You must provide a valid account number to be added. Please contact your Sales Representative or Account Administrator if you don’t know your Account Number.
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
The current password entered does not match your password or new password is the same like one of the previous or password changed last 30 days.
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
This item is discontinued, but you may order against the remaining inventory. You have requested {4} items of the total remaining quantity of {2}.
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
You have no products selected for comparison. Please select at least two products to compare using the 'Add to Compare' checkbox found on product list pages or product detail pages.
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
BROW,DUR,FJ,GRVG,HUBC,JAURE,KOPF,MS,MCGI,MW,MORS,ROLW,SLMS,SP,ADDX,AG,BERG,BH,CAR,CES,CNTA,DURA,EFLX,FALK,HIGH,KRO,LINK,MAR,MB,MCC,OMEG,PSI,REX,RPT,SHA,SIM,STE,TAP,THOM,TLK,TRUE,TUF,VIVA,WRAP,LNKB,RXND,MARB