Evergreen EM Motor Support
Read the Evergreen EM motor installation manual
Read the Evergreen EM dual voltage motor installation manual
Evergreen EM motor installation videos
Electrical Connections
2 min
Complete Installation
12 min
The Evergreen EM motor is a universal replacement for the following:
OEM constant torque ECM motors built with the standard 9-terminal plug shown here.
Genteq® models X13, Endura® Pro, Ensite®, Ensite Air and Evergreen EM motors (including models formerly branded GE® or Ge ECM by Regal Rexnord).
US MOTORS® models SelecTech® and RESCUE® SELECT®
Broad Ocean® motors (OEM motors with 24 VAC speed taps).
Evergreen Motor Selection Guide
If the motor you want to replace is not listed above, open the Evergreen Motor Selection Guide to find the correct Evergreen product.Evergreen Product Warranty
This warranty shall expire twenty-four (24) months from first use of the Product or thirty (30) months from date of shipment of the Product, whichever occurs first. Except as stated here, Regal Rexnord standard limited warranty applies. See Terms and Conditions of Sale.
Evergreen EM Product Information
Visit the Evergreen EM motor landing page for more information.
The following are believed to be the trademarks and/or trade names of their respective owners and are not owned or controlled by Regal Rexnord Corporation. Broad Ocean: Zhongshan Broad-Ocean Motor Co., Ltd.; GE: General Electric Company; US Motors, SelecTech and Rescue Select: Nidec Corporation; Apple Store: Apple Inc.; Google Play: Google LLC.