Critical Spares and Recertification for Turbomachinery Couplings
Turbomachinery is Critical Equipment
In the oil and gas, petrochemical, and power generation industries, turbomachinery is considered ‘critical equipment.’ These high-performance machines generally operate at 1,000 horsepower and rotate 3,000 rpm or greater and include all rotating machines whose reliability is essential to plant operations and whose failure or shut down for maintenance results in production loss.
In most facilities, critical plant equipment has a robust maintenance plan in place, precisely because of high out-of-service costs. Maintenance staff will keep track of this maintenance using asset management software, ensuring all necessary equipment records are maintained. If not properly maintained, many of the components that connect to and support critical turbomachinery equipment, such as high-performance couplings, can cause unscheduled downtime.. All the care and attention given to critical items counts for nothing if there is a potential failure to one of these “wear items.”
Turbomachinery Couplings: The Canary in the Coal Mine
Turbomachinery couplings are generally designed for infinite life when they are operated within their rated capacities. However, engineers and operations managers realize that “infinite life” is theoretical and is often different from real life. Changes in operating conditions can impact the life of couplings, reducing their service life. These changes can result in expensive downtime or potentially equipment damage or failure. If a failure is severe or worst case, catastrophic, it can also damage equipment beyond the application in which the coupling is running.
Modern turbomachinery is a highly complex engineering system and at times there are outages, both planned and unplanned. In today’s competitive landscape, there is sometimes a tendency towards getting processes up and running as quickly as possible, and spares are not always top of mind. This is a potential blind spot which, unsurprisingly, can leave operators and end-users without critical spares when they need them most.
Because couplings may be considered a ‘minor’ part of the overall system, they are often overlooked. In reality, they are crucial components and are typically designed to be the weakest link in the train so as to prevent damage to the connected, critical equipment. Because of this, the coupling is often the first item in the train to show signs of damage or distress during an event. Damage to a coupling may also be an early indicator of more significant problems in other equipment. For example, disc pack fretting could result from resonant torsional frequency, while cracks in the outer disc may signal that the coupling is operating under excessive misalignment.
The coupling can therefore be thought of as the ‘canary in the coal mine.’
Causes Of Coupling Wear
There are many factors that contribute to coupling damage. These include:
- Operating outside of design parameters
- Assembly/disassembly and handling damage
- Corrosion
- Contamination
- High temperatures
- Harsh environments
The Importance Of Spare Couplings
With lead times for new couplings typically ranging from 12-16 weeks – or more for larger units – it is recommended to stock spares for all critical equipment in a facility. Not only will this avoid extended downtime after an event, it will also eliminate logistics issues, such as delays clearing customs and ongoing shipping complications as a result of pandemic restrictions. In addition, it will eliminate the temptation to use third party couplings which, while they may be more easily available, do not comply with the original Regal Rexnord design standards and specifications and should be avoided at all costs.
The Consequences Of Not Having Spare Couplings
Recently, a major Louisiana-based LNG facility experienced a coupling failure that resulted in an unplanned shutdown. This occurred because the couplings were running beyond their rated capacity.
It then transpired that the site in question only had a small number of spare couplings, but not the full complement of different sizes for all critical machinery in the train. Crucially, it did not stock a direct drop-in replacement for the damaged coupling. The end user therefore had to reach out globally to the major equipment OEM and Regal Rexnord’s engineering team to find a workable solution.
In the end it was decided to use a similar, but not identical, coupling to get the train back up and running. “Mixing and matching” of coupling components is not recommended, however, and should never be done without consulting Regal Rexnord. Luckily for the end user, the Regal Rexnord engineering and field service teams found a workable solution within a few days to get the site operational and running at full power.
If a direct drop-in replacement had been available, it would have taken a single shift to complete the changeover with no involvement from major equipment OEMs or coupling manufacturers. Luckily in this case, fitting the alternate spare – and working on an expedited basis - only took a few days resolve. If there had been no spare couplings at all, the start-up delays could have taken up to 16 weeks.
Coupling Recertification
Are you ensuring that your power equipment stays in peak operating condition and minimizing the costs of unplanned downtime, replacement parts and emergency labor with coupling recertification? Learn how recertification can help you!
Learn MoreIn addition to stocking spare couplings, many operators are now also choosing to utilize Regal Rexnord’s recertification process, which brings used couplings back to “as new” by addressing any damage that has occurred while in operation, including issues that may not be visible with the naked eye.
If any damage is found during the recertification process, modifications can be made to the coupling design to help mitigate future risks and improve the operation of the equipment. Changes can also be made during installation to make corrections or adjustments to how the equipment is run.
To assess the extent of the damage and spot any cracks during recertification, the coupling is disassembled and a complete mechanical and metallurgical evaluation is undertaken and documented in an analysis report. This is followed by a glass bead blast (or equivalent) cleaning process to remove any rust or stains on the coupling. All hardware, including disc pack, bolts, nuts, washers and shims are replaced and the coupling is reassembled per the original factory specifications. The coupling is then rebalanced for optimum performance.
If anything is found during the inspection or if plans exist to modify the equipment, the coupling can have updates or modification made to it. New parts can be fabricated and replaced within the coupling assembly to not just recertify, but upgrade.
How Coupling Spares and Recertification Work Together
Spare couplings play an important role in minimizing downtime. With over 90% of returned couplings being candidates for recertification, even if a site decides to purchase new, we recommend that the replaced coupling be recertified for future use as a spare.
A coupling taken out of service during unplanned downtime can affect how fast a plant is able to get back up and running. Though
coupling recertification lead times are about half the lead times of buying new, recertifying couplings during planned downtime means that the Regal Rexnord certified coupling service provider can recertify your coupling and keep you on schedule.
More and more operators and end users these days choose to use the main and a spare model along with our recertification service for couplings. When an outage occurs, the main coupling is replaced with the spare and the main coupling is returned to one of our global Regal Rexnord facilities for recertification to the original design and requirements. Once this is complete, the recertified main coupling is returned to the site to become the new spare for that powertrain. In the event of a future outage that requires a coupling replacement, the cycle is repeated again.
Which Couplings Can Be Recertified?
Recertification is done for most high-performance couplings. Couplings sent for recertification typically come from plants in the oil and gas industries, such as ethylene plants, petrochemical plants and refineries.
Since these are high-performance couplings that must be manufactured, assembled, and balanced with precision, recertification is a factory-provided service and should not be attempted by customers.
By always stocking the right number and sizes of spare couplings, and using a recertification service, end users and plant operators can ensure peace of mind while taking a proactive approach to protect their business. This means no surprises and reduced expensive downtime.