How a Drive-and-Motor Combination Can Power Your Route to Net Zero
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
  2. Regal Rexnord Insights
  3. Drives and Motors Power Route to Net Zero: How Variable Frequency Drives Save Energy
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
Drives and Motors Power Route to Net Zero: How Variable Frequency Drives Save Energy

Edit

Photo of Carbon Dioxide monitor with dial pointing to spot near zero percent mark.


Did you know that many motor-driven systems waste energy? Across various industries, these systems often don't run at optimal efficiency. In some cases, energy losses can range from 20 percent to 50 percent . The level of inefficiency varies across different sectors. Manufacturing, HVAC, water treatment, and pumping systems tend to have more inefficiency. The motors in these systems do not always work at optimal levels.

The world is undergoing a transformative environmental shift. Manufacturers and industry are moving towards sustainable practices that reduce carbon emissions. Countries and industries strive to reach net zero. That's the attempt to cut greenhouse gas emissions as close to zero as possible. The effort is not easy. Reaching net zero requires a complete transformation of how people around the world produce, consume, and move.

At the 26th UN Climate Change Conference, world leaders committed to cut carbon emissions by 2030 and achieve net zero by 2050. But achieving net zero won't be possible without consumers and producers. This transformation involves optimizing the energy efficiency of motor-driven systems. These systems are integral to our modern lives.

One way for industries to achieve net zero is to make motor systems more efficient. One way to do this is to use variable frequency drives (VFDs). VFDs can cut energy use by nhancing the performance of motors and reducing energy consumption.

Understanding Variable Frequency Drives

Variable frequency drives (or adjustable speed drives) control the speed and torque of a motor. VFDs adjust the frequency and voltage of the power supplied to the motor. By varying the frequency and voltage, VFDs enable precise control over motor speed. This allows the motor to match the required load and optimize energy consumption.

Efficiency Gains Through Variable Frequency Drives

Traditional electric motor systems usually run at a fixed speed, regardless of load. This means that the motor is always running at full speed, even when the load is lower or fluctuating. Running a motor at a constant speed wastes energy. If the motor does not have a full load, it may be operating at a level that exceeds the actual demand. This causes unnecessary energy use. By adding a VFD, operators can enhance their motor’s energy efficiency.

Variable Frequency Drives and Speed Control

VFDs give users precise motor speed control. Users can match speed to the actual current requirements. Motors with VFDs only consume the necessary amount of energy, reducing energy waste.

Variable Frequency Drives and Energy Savings

VFDs adjust the motor speed to match the load. This eliminates the need for throttling and mechanical control methods that waste energy. Using lower speed when full power is not needed means large energy savings.

Variable Frequency Drives Allow for Soft Start and Stop

With a VFD, a motor can start and stop gradually. This eliminates sudden jolts and reduces mechanical stress. This feature can extend a motor's lifespan and contributes to energy efficiency. Traditional motor systems experience high inrush currents during startup. VFDs can help avoid this, saving energy and minimizing wear and tear.

How Variable Frequency Drives Enable Net Zero Goals

Using VFDs with a motor aligns with the broader goal of achieving net zero carbon emissions. By reducing energy use and optimizing efficiency, VFDs contribute to a greener future:

  • Carbon Footprint Reduction. Decreased energy consumption translates into reduced greenhouse gas emissions. This is vital in combating climate change and meeting sustainability targets.
  • Renewable Energy Integration. VFDs can make it easier to integrate of renewable energy sources, like solar and wind. By controlling speed and output, VFDs synchronize energy generation from renewables with variable energy demands. This further promotes the use of clean energy sources.
  • Demand Response and Grid Stability. VFDs are flexible enough to adjust operation based on electricity demand and grid conditions. By participating in demand response programs, consumers with VFDs can support grid stability. This also contributes to the efficient use of electricity resources.

LEESON: The Industry Leader in Variable Frequency Drives

As consumers, we have the power to drive the transition to a sustainable and net-zero future. Adopting VFDs in motor-driven systems is one way to do so. We can enhance energy efficiency, reduce carbon emissions, and contribute to a greener planet. LEESON® VFDs  provide precise control over motor speed. This enables optimal performance, reduced energy consumption, and the integration of renewable energy sources. Embracing this technology is a vital step towards achieving net-zero goals and building a greener planet.

Make Your Whole System Energy Efficient

To increase energy efficiency, pair a LEESON® VFD with a SYMAX® permanent magnet motor above IE4, or 90 percent efficient. To learn how LEESON solutions can help you achieve net zero, contact an expert today.



Talk to Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business.