ECM Motor Fan and Blower Innovation | Regal Rexnord
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
  2. Regal Rexnord Insights
  3. ECM Motor Fan and Blower Innovation
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
ECM Motor Fan and Blower Innovation

Edit

Sustainable Building Solutions 

A sustainable design was at the core of Shanghai Tower’s development. From the outset, the design team targeted LEED Gold and China 3 Star ratings. The goal of the designers was to create an architectural jewel that is as efficient as it is beautiful. The building incorporates wind turbines to high efficiency ECM BLDC motors. 

Commercial HVAC Innovations

  • Gripnotch® V-Belts
  • NEMA Premium® Motors
  • AC Drives
  • MVP Sheaves
  • ECM Fan Motors
  • PMAC Radial Flux Motors
  • HubFlex® Shaft Couplings
  • Split Taper Bushings
  • PMAC Axial Flux Motors
  • Variable Speed Motors

HVAC

Leading Edge Technology that Solves Problems 

We offer an array of exceptional solutions for the commercial HVAC industry. Our innovations include: High efficiency NEMA and IEC fan and blower motors, ECM technology for fans, and synchronous belt drives that reduce slippage, belt stretch, and metal to metal contact. PMAC integrated motors provide IE4 efficiencies for a myriad of commercial HVAC applications.


Our Genteq® ECM® X13 motors and blowers were selected for the Shanghai Tower’s VAV system by TROX, an HVAC OEM. After passing TROX’s strict testing benchmarks, and meeting the sustainability standards used by the project consultants, the green light was given.


Over 1,400 Genteq® ECM X13 motors contribute to the increased cooling efficiency of the iconic building’s HVAC system. These variable speed, high efficiency motors with efficiencies, that approach 80%, continue to be the building’s workhorse, providing ongoing savings. 

Value Proposition

We have a developed reputation for conservative motor designs, highly engineered motion control, and power transmission products used in a vast array of commercial and industrial applications around the globe.

Market leading solutions that reduce energy consumption, improve process throughput, provide sustainability, increase productivity, and uptime are at the heart of what drives our world.

High efficiency mechanical solutions are at the cutting edge of what we do best. We are recognized for producing reliable solutions that solve problems in critical applications where performance is crucial.

System Plast is a world leader in conveyor systems and components that reduce energy consumption, improve sustainability, and increase throughput in material handling, bottling, and conveyors.

Our expertise goes beyond just product engineering to include a deep understanding of your applications so that together we can apply the best solutions to optimize your product design, reduce overall cost, and increase your equipment's performance.

As one of the undisputed global leaders in BLDC, PMAC radial and axial flux technologies, bearings, controls, couplings, drive components, gearing and conveyor systems, we deliver exceptional solutions to industries such as Aerospace, Aggregate, Agriculture, Air Moving, Automotive, Beverage, Cement, Commercial HVAC, Compressor, Crane and Winch, Marine, Material Handling, Mining, Oil and Gas, and Pumping.

*NEMA and NEMA Premium are trademarks of National Electrical Manufactures Association. All Rights Reserved.



Talk to Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business. 

Associated Brands

Genteq Logo
Leeson Logo
Century Logo
Browning Logo
Seal Master