How to Use Less Pool Chemicals with a Variable Speed Motor
Owning a pool is a dream come true for many homeowners. But what many don’t realize is that the costs of owning a pool can quickly add up. The average cost of maintaining a swimming pool can be more than $1,800 each year. One fourth of that expense is dedicated to the cost of pool chemicals. How can you keep pool water clean without cleaning out your wallet each month? A great way to start is by using less pool chemicals with a variable speed motor.
Algae Won’t Grow, Even With a Slower Flow
Chemicals play an important role in maintaining the cleanliness and hygiene of pools. Chlorine, pH adjusters, algaecides, and other chemicals sanitize the water, prevent algae growth, and maintain proper water balance.
Traditional pool pumps usually operate at one speed, running at maximum capacity even a lower flow rate would be enough. This constant speed leads not only to excessive energy consumption but also unnecessary chemical usage.
On the other hand, quality variable speed pool pump motors such as the VGreen Evo® motor keep water circulation in check, even during slow flow times. They do this by adjusting the power of the motor to the needs of the system. For times of high use, a variable speed pool pump motor will work harder to distribute the chemicals needed to keep algae and bacteria at bay. During downtimes, a variable speed pool pump motor will slow the required flow, using less of those pricey chemicals while still maintaining a clean environment.
Losing Pool Chemicals Through Water Features
Did you know the average swimming pool loses a quarter of an inch of water each day, just from standard evaporation? Water features such as bubblers, bowls, and fountains can escalate that evaporation, leading to less pool chemicals and more money for maintenance.
But don’t cut off that gorgeous cascade just yet! Pump motors also power these features. By programming a variable speed pool pump motor to cut back on water feature usage during your pool’s idle times, more of the costly chemicals stay in the water.
Turn Down the Turnover Rate
A pool’s turnover rate is the time it takes for all the pool’s water to circulate through the filter system. A variable speed pool pump motor can lessen the turnover rate to only what is needed depending on usage. This cuts back on unnecessary cycles, and keeps those chemicals in the water and working.
Keep more chemicals in the pool by selecting a variable speed pool pump motor such as our reliable Century® VGreen Evo motor today!