Durable Bearing Solutions for Tough Forestry Applications | Regal Rexnord
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
  2. Regal Rexnord Insights
  3. Durable Bearing Solutions for Tough Forestry Applications
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
Durable Bearing Solutions for Tough Forestry Applications

Edit

Forest Banner


 

The forest products industry is tough on bearings. Heavy loads, strong vibration, harsh weather, and constant contamination all shorten bearing life. Because of these conditions, bearings must be durable, stable, and easy to maintain.

Rexnord builds solid housed spherical roller bearings to handle these challenges. A two piece outer ring design gives them several advantages compared to other brands. Rexnord bearings offer:

  • higher load ratings,
  • improved misalignment capability,
  • and the ability to adjust internal clearance quickly in the field.

Together, these features help increase uptime, reduce failures, and extend bearing life.

Here are a few ways Rexnord bearings perform in real forestry environments.

Managing Heat and Load in Drum Chipper Bearings

Drum chippers put extreme stress on bearings due to high speeds and heavy loads. Rexnord spherical roller bearings offer a clear benefit in drum chippers. When needed, operators can increase internal clearance. This reduces operating temperature and helps the bearing last longer.

Reliable Bearing Solutions for High Vibration Stump Grinders

Stump grinders expose bearings to heavy and constant vibration. Rexnord’s press fit outer races help prevent the outer ring from spinning inside the housing, one of the main causes of early bearing failure.

Other design features also matter here, including:

  • Steel retainers, which withstand strong vibratory forces.
  • Face locked threaded covers. These let operators adjust clearance while keeping the bearing secure inside the housing.
  • A locking method that prevents the threaded cover from loosening during vibration.

These features work together to protect internal components and improve reliability.

Protecting Bearings in Chippers, Grinders, and Debarkers

Some equipment needs the opposite approach. Log debarkers run at lower speeds but still generate high vibration. In these cases, operators often decrease internal clearance. Reducing this gap shortens the travel distance between rolling elements and the raceway surfaces. This helps prevent “roller slap.”

Heavy vibrations cause roller snap. Roller slap occurs when rollers bounce between the inner and outer ring raceways. This impact creates stress inside the bearing, leading to increased wear and possible early failure. By tightening clearance, operators can significantly reduce this risk.

Bearings Built for Harsh Forestry Conditions

Forestry equipment puts extreme stress on bearings. Whether the task involves chipping, grinding, debarking, or general material handling, these machines push components to their limits. Rexnord solid housed spherical roller bearings can handle high heat, heavy loads, and strong vibration. Rexnord bearings are a trusted choice in demanding forestry environments.

For more information, learn about Regal Rexnord’s industry leading bearings products.

Frequently Asked Questions About Bearings in the Forestry Industry

Where can I find bearings in forestry equipment?

Many parts of the forestry process use bearings. This includes: conveyors, infeed systems, sorting equipment, debarkers, chippers, sawmill machinery, and finishing equipment.

What conditions make the forestry industry so challenging for bearings?

Forestry puts heavy stress on bearings. They face high loads, strong vibration, heat from nearby processes, and constant contamination. Outdoor environments add even more wear. If bearings are not built for these conditions, their service life can drop quickly.

Why are sealing and contamination resistance important in forestry?

Forestry equipment operates around sawdust, bark, mud, moisture, and other debris. These contaminants can enter the bearing and break down lubrication. Strong sealing helps keep debris out so the bearing stays protected and runs longer.

Why is adjustable internal clearance important?

Forestry machines create different levels of load and vibration. Adjusting internal clearance helps manage heat, reduce stress on internal parts, and improve overall stability. It also helps prevent problems like roller slap.

What is “roller slap,” and how do these bearings help prevent it?

Roller slap happens when the rollers bounce between the raceways during vibration. This impact can cause heavy wear and lead to early failure. Reducing internal clearance shortens the distance the rollers can travel. In machines like debarkers, this helps prevent slap and protects the bearing.

How do Rexnord solid housed spherical roller bearings improve performance in forestry applications?

These bearings use a two piece outer ring design. This design supports higher load ratings and better misalignment handling. It also lets operators adjust internal clearance quickly in the field. Together, these features help increase uptime and extend bearing life.



Talk to Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business. 

Mike Martin

Mike Martin

Mike is an Application Engineer for Rexnord's Bearing Division. Since 2014, Mike has been with Regal Rexnord within the Bearing Application Engineering Group. He provides customers' with support such as helping them select the proper Bearing, onsite assistance, maintenance and installation training, and troubleshooting with any issues.

Page Updated: March 20, 2026