A Technician’s Guide to Safely Handling Industrial Motors | Regal Rexnord
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
  2. Regal Rexnord Insights
  3. A Technician’s Guide to Safely Handling Industrial Motors
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
A Technician’s Guide to Safely Handling Industrial Motors

Edit

Photo of chain with lifting hook.


Industrial motors are essential parts of the manufacturing processes. The sizes and horsepower ratings of these motors can vary. Yet they all have something in common: their size and weight can be a challenge when it comes to safe handling and installation.

Technicians should follow proper procedures when handling motors. It's important to use appropriate equipment and techniques to prevent accidents and injuries. These procedures will ensure the safety of people and equipment. Here are some best practices for moving and installing heavy industrial motors.

The Risks of Improper Motor Handling

Attempting to move heavy industrial motors without the right equipment and techniques can have grave consequences. You could damage the motor and pose a a significant risk to the safety of personnel involved in the process. Mishandling can result in dropped or uncontrolled motor movements. This can lead to injuries, property damage, and even fatalities. It is crucial to approach motor handling with a well-defined plan and the right tools.

Step 1: Planning the Lift

Before attempting to move an industrial motor, careful planning is essential.

Start by assessing the weight and dimensions of the motor. This will help you determine the appropriate lifting equipment for each stage of the process. During planning, consider the motor's path from its current location to the installation area. This should include any obstacles or challenges along the way.

Step 2: Choosing the Right Equipment

Distinct stages of the motor handling process require specific lifting equipment. A manual boom or A-frame might be ideal for controlled lowering. During transporting the motor, a motorized lift truck could be the best choice. Avoid using building structural members for lifting. Parts of the building structure may not be designed to handle the load and could pose a safety risk.

Step 3: Selecting the Right Securing Devices

Properly securing the motor is critical to prevent movement during handling. Identify the appropriate straps, hooks, and other devices for each stage of the process. Ensure that the chosen devices are rated for the weight of the motor and are in good condition. Regular inspections of lifting gear are essential to guarantee their integrity and functionality.

Step 4: Ensuring Proper Positioning

One of the most challenging aspects of motor handling is maintaining control over its position. Leveling equipment can ensure the motor remains stable during lifting, carrying, and lowering. Use shims or wedges to make necessary adjustments to the motor's position.

Step 5: Collaborative Execution

Industrial motor handling is rarely a one-person job. Effective communication and collaboration among the team members involved are crucial. Assign specific roles to each team member, such as the operator, signaler, and supervisor. These roles can ensure a smooth and controlled operation.