What Do Thermal Protectors and Resets in your Motors Mean?
Many industries rely on electric motors to keep operations moving. From factory floors to everyday machines, motors power essential processes. But when an electric motor is overworked, it can overheat. And that can lead to catastrophic motor failure. Overheating can lead to costly downtime, equipment damage, and even safety hazards. Fortunately, thermal protectors within an electric motor can prevent overheating.
Thermal protectors shut down a motor's operation when it gets too hot. These important safety measures can deliver peace of mind for customers and prolong motor life expectancy.
How Does Heat Affect Motors?
In many applications, heat is the greatest danger to a motor. Heat can wear down grease and bearings and destroy insulation.
What Are Some of the Causes of Motor Overheating?
Overheating doesn’t happen without a reason. Here are some frequent causes:
- Overloading: When a motor is asked to deliver more power than it was designed for, it draws extra current. This creates heat that can quickly push the motor beyond safe limits.
- Poor Ventilation: Motors need airflow to stay cool. Dust buildup, blocked vents, or operating in confined spaces can trap heat and lead to overheating.
- High Ambient Temperature: If the surrounding environment is too hot, the motor can’t shed heat effectively. This is common in settings without proper cooling systems.
- Incorrect Motor Sizing: Using a motor that’s too small for the job forces it to work harder than intended, increasing heat and stress.
- Voltage Imbalance or Low Voltage: Electrical issues like low voltage or phase imbalance make the motor inefficient, causing it to run hotter than normal.
- Continuous Duty Without Rest: Motors designed for intermittent use can overheat if they run without downtime.
- Mechanical Issues: Worn bearings, misalignment, or excessive friction in connected equipment can make the motor work harder, generating extra heat.
What is Thermal Protection and Why Is it Important?
Thermal protectors (also called overload devices) are built-in safety features. They “trip” or stop the motor when it overheats or is overloaded.
Why does this matter? Without a thermal protector, an overheated motor can fail, costing time and money. Worse, it can create safety hazards for workers and equipment.
Safety Considerations for Thermal Protectors
Here are some safety tips to keep in mind regarding thermal protectors on your motors:
- Warning: Never bypass a thermal protector because of nuisance tripping. Frequent tripping usually means something else is wrong; like overloading or poor ventilation. Fix the root cause of the nuisance (or false) tripping instead.
- Never use an automatic reset protector in applications where a sudden restart could injure someone. In those cases, use a manual reset protector.
- Don’t keep resetting the motor while it’s hot. This can damage both the motor and the protector. Always wait until it cools.
How Thermal Protector Resets Work
Thermal protectors cut power when the motor overheats. Once the motor cools down, the protector resets. There are two types:
Automatic Resets
These restore power automatically after the motor cools. They’re convenient, but they can be dangerous if an unexpected restart could hurt someone. Avoid using them on equipment like saws, compressors, or conveyors.
Manual Resets
These require you to press an external button to restart the motor after it cools. If the motor is still too hot, the protector will trip again. Manual resets are safer because they prevent surprise restarts. They’re best for hazardous applications like compressors or cutting machines.
The choice between automatic and manual reset depends on the application and safety requirements.
Use Thermal Protectors to Protect Your Equipment
Protecting your motor from heat and overload is critical for safety and the longevity of your equipment. If your thermal protector trips often, it’s a sign of a bigger problem. Check your motor specifications, application, and environment before installation.
Need help seeking the right thermal protector for your application? Contact one of our experts below for more information.
Talk to Our Sales Team
We're here to help. Our team of experts is ready to help energy-efficiently power your business.
Page last updated: December 4, 2025