What NEMA Frame Size Can Tell You About Rigid Base Motors
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
  2. Tools & Resources
  3. Training
  4. Motor Mastery University® Training
  5. Motor Minute™
  6. What Does NEMA Frame Size Tell You About Rigid Base Motors
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
What Does NEMA Frame Size Tell You About Rigid Base Motors

Edit

Motor Mastery Logo
Motor Mastery University®


Video Library
Video Library


Literature Library
Literature Library


Podcasts
Podcasts


Articles
Articles


Articles
Motor Minute™


Online Learning
Online Learning


Face-to-Face Education
Face-to-Face Education

July 16, 2024


Motor Minute™ Technical Tip – What Does the NEMA®* Frame Size Tell You About Rigid Base Motors?

Hi, Chris from Regal Rexnord here with your Motor Minute technical tip. Helping you become an HVAC motor pro one minute at a time.

Today’s Motor Minute topic is NEMA frame sizes and rigid base motors.

The NEMA frame size directly correlates to the dimension between the center of the shaft in the motor and the mounting base. The reason this dimension is so important is to ensure that the replacement motor shaft will be in the same location as the original motor.

It is important to note that the NEMA frame dimensional standards correlate to a motor with a rigid base (also referred to as base mount or foot mount). This means that the mounting location of the motor in relationship to the center of the shaft is a fixed dimension.

In the NEMA frame dimensions chart, the letter (D) denotes the center of the shaft dimension. The numbers in the frame size are part of a mathematical equation that correlates to this dimension.

nema frame chart
nema frame dimension illustration

T-Frame Motors Built With a Rigid Base

The first two digits of the frame size divided by four (4) equals the center of the shaft dimension. For example:

  • 145T (14 divided by 4 = 3½” shaft height)
  • 215T (21 divided by 4 = 5¼” shaft height)
T frame motors chart

48 and 56 Frame Motors Built With a Rigid Base

The two digits of the frame size divided by sixteen (16) equals the center of the shaft dimension. For example:

  • 48 (48 divided by 16 = 3” shaft height)
  • 56 (56 divided by 16 = 3½” shaft height)
48 and 56 frame motors chart

The frame size of rigid base motors also denotes the dimensions (location) of the mounting holes in the base.

  • The letter (E) denotes the dimension between the mounting holes and the center of the shaft.
  • The letter (F) denotes the dimension between the mounting holes and the center of the base.
rigid base motors chart
rigid base motors parts

To summarize, the NEMA frame size in rigid base motors denotes the dimensions of:

  • the center of the shaft to the base
  • the mounting holes in the base
nema frame size chart
single phase only chart

For the replacement motor to match the location of the existing mounting holes and the center of the shaft of the motor being replaced, the frame size is crucial.

When selecting a replacement rigid base motor, the frame size is just as important as the electrical ratings but is often overlooked and widely misunderstood.

And that’s a wrap on this segment of Motor Minute technical tips. Remember that we provide motor training and product information in multiple formats including videos, literature, podcasts, articles, of course Motor Minute technical tips and classroom education both online and face to face. All of this industry leading training is available at no charge to HVAC professionals at regalmmu.com. Thank you for taking the time to build your motor knowledge.


*NEMA is the trademark of the National Electrical Manufacturers Association and is not owned or controlled by Regal Rexnord Corporation.





HVAC Motor Solutions mobile app logo

Additional Motor Minute Tech Tips

Download the HVAC Motors Solutions mobile app for additional residential HVAC contractor tools and resources.

Download on the App Store
Get it on Google Play