You Can Become a Motor Master - Constant Torque Motors | Regal Rexnord
You Can Become a Motor Master - Constant Torque Motors (Part 2 of 4)
December 22, 2023 (21:50 in length)
If you want to be an ECM expert, you are in the right place.Constant torque ECM indoor blower motors were introduced to the HVAC industry in 2006. Today these motors have displaced PSC motors as the most widely used indoor blower motor technology in new residential and light commercial HVAC systems today.
Constant torque ECM motors were introduced as simple 5 speed motors. However, today they are also built with multiple communication options similar to their constant airflow ECM cousins.
This training covers the HVAC applications constant torque motors are found in, how they are operated, how to adjust airflow for performance and longevity, and how to diagnose and replace with either OEM motors or universal Genteq® Evergreen® EM motors.
This is not just a high level overview. This is training you can use in the field on your next job. It’s time to get comfortable with ECM motors and become an expert at operating and diagnosing HVAC systems with constant torque motors.
ECM motors are not a fad. They are already the most widely used motor technology in new residential and light commercial HVAC systems today. Whether you have been on the job 20 days or 20 years, you will be glad you listened to this podcast.
Learn more about Regal Rexnord's FREE training at www.regalmmu.com.
For more information on the "Did You Know" program and other resources from ESCO, please visit the HVACR Learning Network.