How EC Motors Work | Motor Mastery University
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
  2. Tools & Resources
  3. Training
  4. Motor Mastery University® Training
  5. Podcasts
  6. How EC Motors Work
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
How EC Motors Work

Edit

How EC Motors Work

April 1, 2021 (47:49 in length) 

In this podcast episode, Bryan and Chris Mohalley from Regal Rexnord discuss EC motors. They also describe ECM applications and how those motors work.

EC motors (ECMs or "ECM motors") are electronically commutated motors. These motors are generally three-phase AC motors operated by a drive; that drive is a combination of an AC-to-DC converter, microprocessor, and frequency drive. So, the frequency delivered to the motor is generated electronically.

When it comes to inputs, the ECM works like a printer. One input provides power (from the wall to the printer). The other cable tells the printer what to do and when to do it (from the computer to the printer). An ECM will have a line voltage connection and a constant 24v communication input. Constant-torque ECMs work like PSC motors in the way they use control taps; other ECMs may use DIP switches.

ECMs are direct-drive motors that differ from PSCs because they don't have a capacitor. EC motors also have a permanent magnet, which can affect diagnosis if you rarely come across indexing.

AC motors use magnetism; when you pass energy through the stator coil, the coil creates an invisible magnetic field, which then induces a magnetic field into the rotor. When the rotor picks up a magnetic effect, it starts to spin. EC motors have that magnetic effect in their magnets.

Chris and Bryan also discuss:

  • Regal Rexnord's history and brands
  • Effectiveness of metaphors and acronyms in our industry
  • Constant-torque ECM vs. variable-speed motor
  • Motor modules
  • Changes to the ECM design over time
  • ECM manufacturers
  • Three-phase power and controls
  • Reading ohms
  • Glued-on vs. slotted magnets
  • RPM and the effects of poles and frequency of power delivered

Learn more about Regal Rexnord's FREE training at www.regalmmu.com.

Learn more about the HVACR Training Symposium or buy a virtual ticket today at https://hvacrschool.com/symposium.

If you have an iPhone, subscribe to the podcast HERE, and if you have an Android phone, subscribe HERE.