Our “Extreme” Solution for Food Processing Protection | Regal Rexnord
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
  2. Regal Rexnord Family of Brands
  3. LEESON® Motors
  4. Our “Extreme” Solution for Food Processing Protection
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
Our “Extreme” Solution for Food Processing Protection

Edit
Photo of man washing down machinery.

 

Poultry processing is one of the largest segments of U.S. agriculture, generating billions of dollars in revenue every year. New concerns around cleanliness, health, and food quality are expected to create heavy growth within the segment.

Regulations and health standards are stringent when it comes to animal product consumption. Contaminants and potential downtime pose dangerous and expensive threats to poultry processing. The machinery used must be of the highest quality to easily blend into the standards and safety practices imposed on these operations.

Building the Best Product Portfolio for Customers

One of our distribution customers offers a variety of products impacting applications such as poultry across the country. Their presence in this segment allows them to supply crucial and in-demand products that influence consumers at every stage of the value chain.

Whether it be stainless steel bearings for added protection within washdown environments, beverage hoses with protective layering to avoid bacteria build up, or electric motors with varied degrees of washdown protection, can support businesses. For decades this distributor has been committed to driving out cost and time efficiency up for their customers. However, finding safe and efficient machinery for poultry processing is easier said than done.

Securing reasonably priced machinery for a business is one thing but that must be balanced with ensuring downtime in the future also can be avoided or minimized.

Choosing the Right Washdown Product

Working with the distributor, we learned about their concern over downtime and motor replacements in poultry processing environments. We know replacing a motor in production is imminent, but reducing the frequency of those replacements can be helped with quality products.

Our distribution customer faced concern over stocking washdown motors that balanced protection against high-pressure sanitization and operational efficiency. With the amount of cleaning products in poultry processing, it is common for motors to face water and chemical contamination or ineffective sanitation that leads to bacterial buildup. Without the proper motor and ingress protection, equipment is more prone to breakdown.

With potential downtime of great concern, the distributor needed a solution that would extend the life of equipment in production. One hour of unplanned downtime costs a processing facility anywhere between $30,000-$50,000. Anywhere they can combat this downtime would allow them to fulfill their goals of driving out cost and time efficiencies up for their customers.

Not Your Ordinary Washdown Motor

A sale representative agency of Regal Rexnord worked with the distribution customer to find a motor solution that would withstand harsh conditions that many motors deal within poultry processing applications. After careful consideration, the sales team introduced the LEESON® Extreme Duck® Ultra motor to the distributor.

This was not only a motor that withstood washdown, but it offered full stainless-steel encapsulation with the highest ingress protection (IP) on the market, an IP69K rating. That made it the perfect candidate for washdown environments the distributor supplies product to. Greater exterior and insulation protection would inherently lead to motor longevity, but that is not all from the Extreme Duck® Ultra.

Another notable feature for this LEESON® motor includes market-defining Q-Car™ rotor cartridge. This removable rotor cartridge allows technicians to easily access the interior of the motor, replace worn bearings, and return the motor to production in under 10 minutes with IP69K rating intact. The Extreme Duck® Ultra motor not only offers protection against external contaminants, but it delivers a solution for inevitable issues like bearing wear and tear.

With a product like the Extreme Duck® Ultra, the distribution customer was able to deliver a high-impact solution to their customers that saved time and resources otherwise lost due to downtime.

Regal Rexnord’s Washdown Solutions

Regal Rexnord manufacturers durable products that make a difference within food processing applications such as poultry processing. Thanks to our extensive range of washdown motors, we can deliver solutions for any washdown requirement.

Products like the LEESON® Extreme Duck® Ultra motor can revolutionize your business and applications. With unmatched protection and innovation, the Extreme Duck® Ultra motor keeps what is outside – out.

 


Talk to one of our expert sales professionals about how our solutions can efficiently power your business.