The Extreme Duck® Ultra Motor Does It Again
The LEESON® Motor brand once again delivers superior protection and sustainability for retail and commercial end users.
Industry
The fresh food packaging industry is a colossal $123.4 billion market, with projections indicating a 5% growth over the next decade. This means nearly $130 billion will be dedicated to packaged fruits and vegetables globally. With intense competition to deliver the freshest products, companies can hardly afford the risks of machine downtime or, worse, food contamination. As a result, durable and reliable equipment is crucial for businesses to maintain non-stop production.
Problem and Solution
A leading North American producer of salads and fresh foods faced significant issues with their legacy stainless steel motors. These electric motors were costly and only lasted six months, making their cost of ownership unsustainable.
Regal Rexnord, in collaboration with Applied Industrial Technologies, introduced the LEESON Extreme Duck® Ultra motor, featuring the innovative Q-Car™ rotor cartridge. Beyond its impressive IP69 rating, the motor’s removable and replaceable rotor cartridge received high praise from the customer. In less than ten minutes, a technician can replace the rotor cartridge on the production line without compromising the motor’s IP69 rating. At just a third of the cost of a new motor, this feature offers substantial savings in time, money, and disposal resources.
Application
With the Extreme Duck motor's IP69 rating, the company can confidently perform their sanitation procedures without worrying about motor damage. This allows for seamless integration into the existing production line and ensures the motors can withstand the rigorous cleaning processes necessary in food packaging facilities.
Solution Type
The Extreme Duck Ultra motor represents a sustainable and cost-effective solution. Its key feature, the Q-Car rotor cartridge, allows for quick and easy maintenance, reducing downtime and operational costs. This innovation aligns with the industry's need for reliable and durable equipment.
Product Description
The Extreme Duck Ultra motor is designed to deliver exceptional performance in harsh environments. It features an IP69 rating, ensuring resistance to water and dust ingress. The standout feature is the Q-Car rotor cartridge, a removable and replaceable component that simplifies maintenance and extends the motor's lifespan, offering a cost-effective alternative to complete motor replacement.
Impact
Since implementing the Extreme Duck motor five years ago, the company has rebuilt the motors five or six times, resulting in significant cost savings compared to their previous motors. The low cost of ownership allows businesses like this one to reinvest in their production equipment, positively impacting their bottom line. Following the success of the Extreme Duck, the company plans to expand its use to other applications within their plant.
To discover how the Extreme Duck Ultra motor and its Q-Car rotor cartridge can benefit your facility, contact our experts today.