How to Select the Right Replacement Motor for a Commercial Oven
Take it from us, takeout in the United States is big business. The U.S. Bureau of Labor Statistics says each year, the average American spends more than $3,500 on dining out. Commercial kitchens prepare many of these meals. Most of these kitchens have specialized equipment, namely, commercial ovens. Whether it's baking to perfection or providing a final finishing crisp, commercial ovens are a vital piece of the commercial kitchen. When these essential appliances break down, a quick and reliable fix is crucial.
Motors are a critical component of the commercial oven. Yet, over time, they are also vulnerable to breaking down. When motors fail, careful consideration is important to finding the correct replacement. In this guide, we've gathered some top tips to help you find the perfect motor for your commercial oven.
The Role of Motors in Commercial Ovens
There are two main types of commercial ovens: radiant and convection. A radiant (or standard) oven utilizes heating elements at the bottom of the unit. These heating elements radiate heat in the interior compartment to cook food. By comparison, these are inexpensive among commercial oven offerings. The drawback: heating food evenly is challenging for radiant ovens.
The other option, convection ovens, combine traditional baking elements with a ventilation fan. The fan circulates heat through the oven cavity, delivering more balanced heating. A specialized electric motor powers the convection oven fan. When this fails, it leaves your oven full of hot air and diminished cooking capabilities.
Selecting a Replacement Commercial Oven Motor
For the easiest way to find a motor replacement, consult the original manufacturer. Equipment manuals usually list the necessary motor specifications. Matching specifications will ensure compatibility with horsepower, voltage, phase, RPM, and frame size. You can use the original motor’s nameplate to help cross-reference potential solutions.
Mounting is crucial, especially for commercial oven replacements. These motors often need specialized mountings like round or round with extended studs. Ensure the replacement motor fits the specific design and mounting requirements. Motor size and shaft orientation are also key factors.
Additionally, commercial oven fan motors are highly specialized for usage in commercial kitchens. A standard electric motor will not fit the bill. To ensure optimal performance, you should consider these key factors:
Enclosure Type
Environmental factors present in commercial ovens present a hazard to motors. Motor enclosures can provide adequate protection against heat, moisture, and debris. Look for enclosure types like TEFC (Totally Enclosed Fan Cooled) or TENV (Totally Enclosed Non-Ventilated). These enclosures can prevent contaminant ingress that could harm a motor.
Temperature Rating
Heat is the number one enemy when ensuring the long-term operation of a motor. This holds particularly true when evaluating replacement motors for commercial ovens. Temperatures in commercial ovens rise to approximately 40° C or higher. High temperatures could lead to overheating or premature failure. Choose a motor able to withstand the high temperatures. Look for motors with high-temperature ratings specifically suited for oven applications.
Safety Requirements
Underwriters Laboratories (UL) and the Canadian Standards Association (CSA) publish standards for equipment safety. Choose a motor that is compliant with these standards. This will ensure your choice has undergone rigorous testing for safety and performance.
Motor Footprint
Space is a premium for many commercial kitchens. Equipment should maximize output while minimizing the necessary footprint. Typical commercial oven motors widen the unit beyond a standard 36” doorframe. Larger equipment makes storage, cleaning, and service difficult. When sourcing a replacement oven motor, seek options that feature compact frames.
Commercial Oven Motor Upgrades
Finally, replacing your commercial oven motor is the perfect time to consider upgrading. Selecting a more energy-efficient motor can cut operating costs and reduce environmental impact. High-efficiency motors can contribute to cost savings over the long term.
Updated technology leads to another enticing motor upgrade. Customizable motor programming offers more efficient operation. Programming can cut costs through more efficient operation and time and simplify processes.
Selecting the right replacement motor for a commercial oven is crucial. You can ensure uninterrupted operation and maintain optimal performance in the kitchen. Commercial ovens play a critical role in food preparation. The appropriate replacement motor can help you continue to deliver quality goods while minimizing downtime and maximizing productivity.
Talk to Our Sales Team
We're here to help. Our team of experts is ready to help energy-efficiently power your business.Motor Solutions for Commercial Ovens
The SyMAX®-SRt motor is a best-bet solution for commercial oven replacement motors. This tethered motor is compact, efficient and leverages smart technology.
SyMAX-SRt reduces the axial length need by a commercial oven motor by 68 percent. This allows an easy-fit through traditional 36” commercial kitchen doorframes. The motor’s variable speed supports noticeable efficiency savings throughout the speed range.
Further, its cutting-edge technology keeps your kitchen connected. SyMAX-SRt features a separate tethered intelligent control enables agile programming capabilities. The SyMAX-SRt delivers a simplified installation and operation experience. Users can see lower cost and higher performance when compared to induction power. For more information, browse our selection of SyMAX-SRt motors.