How to Make Your Heat Pump Water Heater Even More Efficient
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
  2. Regal Rexnord Insights
  3. Making Heat Pump Water Heaters Even More Efficient
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
Making Heat Pump Water Heaters Even More Efficient

Edit

Photo of technician adjusting dial on water heater


People rely on home water heaters for comfort, health, and cleanliness. Most water heaters found in residences are traditional tank water heaters. But in attempt to go green and save on energy costs, many homeowners are turning to heat pump water heaters. Added electric motors give heat pump water heaters an extra efficiency boost. Users find heat pump water heaters can be more cost and energy efficient.

What is a Heat Pump Water Heater?

Traditional water heaters use either gas heat or an electric heating element. The heating element brings water in the tank up to a set temperature before distributing it through the system.

Heat pump water heaters are different. A heat pump water heater takes heat from the space surrounding it and use electricity to move the heat from outside the tank to inside the tank.

Heat Pump Water Heaters Versus Gas/Electric Water Heaters

Traditional and heat pump water heaters rely on different methods to heat water. What are the benefits of using a heat pump water heater?

Gas water heaters can use more fuel to operate but are typically less expensive. Fluctuating electricity rates could put the usage cost of an electric heater higher than gas heaters.

Electric water heaters are the greener option between the two types of traditional heaters.

But when you add heat pump water heaters into the mix, you'll get a different result. Heat pump water heaters are more efficient than traditional water heaters. The U.S. Department of Energy says these systems can be up to three times more efficient than traditional gas or electric water heating options.

Will Switching to a Heat Pump Water Heater Work For You?

Most heat pump water heaters work best in climates that stay between 40° and 90° Fahrenheit. The majority of areas in the United States are outside this range year round. But homes and buildings can in these areas can still reap the benefits of a heat pump water heater. Users can retrofit heat pump water heater onto an existing system for an efficiency boost. With this setup, the existing system acts as a backup.

How Can the SyMAX-PRO Improve Heat Pump Water Heaters?

The LEESON SyMAX-PRO® motor runs efficiently at variable speeds. This pairs perfectly with the fluctuating speed the heat pump needs to keep a consistent temperature. SyMAX-PRO has an integrated electric controller working with an axial fan to ensure the most efficient air flow for your heat pump.

Are you interested in giving your heat pump water heater a big efficiency boost? Or, are you looking for the most reliable motor to provide long-lasting service for your clients? Contact a member of our product team below:

Talk to Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business.